The Raritan Blog

Blazing Virtual Media Speed for the Dominion KX IV - 101

Jessica Ciesla
August 12, 2020

When we talk about the Dominion KX IV -101 as Raritan’s fastest KVM-over-IP switch, we are usually focused on its ability to support 4K video or 1080p video at 60 frames per second. But video isn’t the only area where the KX IV-101 shines!  Due to its all-digital architecture and its direct USB connection to the target computer, the KX IV-101 supports virtual media much faster than our current generation Dominion KX III switches.  


Power Tip #2: Avoid Overloading Phases Within a PDU

Jessica Ciesla
July 23, 2020

While three-phase PDUs provide higher power capacities, they do require planning before server deployment. An unbalanced power draw on one or two of the three phases of the PDU creates stranded capacity which increases wasted electricity. Additionally, this scenario can lead to a cascading failure condition upstream. PX3 PDUs actively monitor balancing between phases and if configured correctly can alert you or your team when phases are unbalanced beyond a certain threshold. As a best practice it is important to have all three phases as balanced as possible to minimize unanticipated disruptions and wasted electricity.


Power Tip #1: Ensure That You Are Receiving Alerts on Critical Events:

Jessica Ciesla
July 15, 2020

Raritan's PX3 PDUs monitor a variety of electrical and environmental parameters. You can receive alerts on anything that gets monitored – inlet data, outlet data, circuit breaker status, unbalanced loads, and power factor, to name a few. To configure and receive alerts successfully, you need to ensure the following actions have been completed: 

1. Configure Alert Delivery Mechanism – how to set up and receive your alerts: SNMP and/or SMTP.

a. If you prefer your alerts to be sent to an SNMP manager tool, you need to enable: Device Settings > SNMP > Enable SNMP Notifications

It is important to note that this setting is different from the SNMP Agent setting. You won't be receiving SNMP alerts even if you have enabled SNMP v1/ v2c if you don't explicitly enable SNMP Notifications.


KVM Remote Management in the COVID-19 Pandemic Era

Jessica Ciesla
June 15, 2020

The COVID-19 pandemic is an evolving world-wide public-health and economic crisis. Companies must keep their business operations and systems running.  They also need to keep their employees safe and healthy.  Many employees are now working from home, either on a full or part time basis. While the worst seems to be behind us in much of the United States, Europe and Asia, the Center for Disease Control (CDC) is warning that there may be a “second wave” in the fall/winter. Remote management can be of enormous benefit in this type of uncertain environment.


The New Dominion LX II: Why You Should Trade Up

Jessica Ciesla
April 2, 2020

Looking for an economical KVM solution? This blog discusses features included in the new Dominion LX II, and why it would be beneficial for you to trade up from the original Dominion LX. 

The new Dominion LX II from Raritan is the latest in a line of products designed with the small to midsize business IP KVM switch user in mind.  Our new unit is designed to provide economical, Java-free, BIOS-level remote access to between 8 and 16 servers as well as virtual media.  The new Dominion also supports connections up to 15 frames-per-second at a resolution up to 1080p and 1200p.  With six different options available, the next generation LX II is poised to become the leading SMB IP KVM switch on the market today.


Page 2 of 85 pages  < 1 2 3 4 >  Last ›